Bulletproof Glass vs. 60,000 PSI Waterjet: Will The Glass Crack Under Pressure?

FunKnowledge
Can bulletproof glass withstand the force of a 60,000 PSI waterjet? In this thrilling showdown, the waterjet takes on a 2-inch thick glass panel. Watch as the nearly indestructible meets the unstoppable in a battle of precision versus power. Who will win?

 

When you think of bulletproof glass, you imagine an impenetrable barrier that can stop high-caliber rounds, protect valuables, and even save lives. But what happens when this nearly indestructible material meets one of the most powerful cutting tools on the planet—a 60,000 PSI waterjet? The answer might surprise you.

 

In a fascinating video showdown, the waterjet takes on a 2-inch thick bulletproof glass panel, pitting sheer water pressure against hardened material designed to withstand gunfire. Spoiler alert: The waterjet doesn’t just cut through the glass—it carves it like butter.

 

The Power of the Waterjet

 

Waterjets are no ordinary cutting tools. They utilize an ultra-high-pressure stream of water, pumped at a staggering 60,000 PSI, which is strong enough to slice through metal, stone, and, yes, even bulletproof glass. This extreme pressure is equivalent to the force of a hydraulic press, but focused into a stream as narrow as .003 inches. When that concentrated force hits a surface, it can produce incredibly precise, clean cuts without generating heat or damaging the material.

 

Industries like aerospace, automotive, and mining rely on waterjets for their versatility and precision. They're especially useful for cutting softer materials that might be damaged by traditional methods. Imagine slicing a piece of fruit into perfect, paper-thin slices without crushing it—that’s the kind of finesse a waterjet can deliver.

 

Bulletproof Glass: Tough, But Not Invincible

 

Bulletproof glass is a composite material made up of layers of glass and plastic, designed to absorb and dissipate the energy of a bullet. It's capable of withstanding high-velocity impacts from firearms like the AK-47, making it a go-to material for security applications. In the video, the glass easily shrugs off 30 rounds of ammo from an AK, but when it’s put under the waterjet, things take a different turn.

 

The waterjet’s stream easily slices through the 2-inch thick bulletproof glass, even carving out a gun shape—a perfect irony. The process demonstrates just how powerful the combination of water and pressure can be, and how even the toughest materials can be compromised under the right conditions.

 

Waterjet vs. Bulletproof Glass: The Verdict

 

So, what’s the takeaway from this incredible demonstration? While bulletproof glass is highly effective against bullets, it’s no match for a 60,000 PSI waterjet. This tool's power lies in its precision and the focused force it can apply, making it one of the most versatile cutting methods available.

 

Who knew water could be so powerful?

 

Find the Perfect CAD Model for Your Project on 3Dfindit

 

Ready to take your designs to the next level? Discover millions of 3D CAD models from leading manufacturers on 3Dfindit.com. Whether you’re an engineer, architect, or designer, you can quickly search, configure, and download exactly the parts you need—all for free. Don’t waste time searching through endless catalogs; let 3DfindIT.com streamline your design process with accurate, ready-to-use CAD models that fit your specifications.

 

Start exploring now and transform your ideas into reality with the power of 3Dfindit.com!