Little BIM/Big BIM – Open BIM/Closed BIM

KnowledgeArchitecture EngineeringGlossaryBIMImportant Content
If you deal with the planning method Building Information Modeling (BIM), sooner or later you will inevitably come across the terms Little BIM, Big BIM, Open BIM and Closed BIM. We explain what these technical terms are all about.

What is Little BIM and Big BIM?

The digital working method Building Information Modeling (BIM) can initially be divided into Little BIM and Big BIM.

  • Little BIM: The technique describes the limited application as an isolated solution within an office or construction company as well as a planning discipline. Mostly, the software of only one manufacturer is used here.
  • Big BIM: This variant refers to the continuous use of digital building models across different trades and lifecycle phases.

What is Open BIM and Closed BIM?

 In terms of software, BIM can be further divided into Open BIM and Closed BIM.

  • Open BIM: Data is exchanged via various software solutions and open, standardized data models. For the exchange of BIM data, the IFC format (Industry Foundation Classes) is the leading international standard. Open BIM offers the advantage that all project participants can choose the software that is best suited to their own work processes.
  • Closed BIM: Data exchange takes place via a uniform program. These are proprietary, closed data models. All planning participants work simultaneously in one building model. Closed BIM enables the uncomplicated coordination of specialist models. By using an identical file format for planning, information losses due to misinterpreted data can be largely excluded.

 

The image illustrates the different approaches and dimensions of Building Information Modeling (BIM) using a quadrant model. It highlights two axes: the openness of data, contrasting open and standardized data models (Open BIM) with proprietary and manufacturer-specific solutions (Closed BIM), and the scope of utilization, ranging from isolated, discipline-specific applications (Little BIM) to comprehensive, cross-disciplinary use of digital building models throughout all lifecycle phases (Big BIM). The message emphasizes that

 

What are the BIM Variants?

There are four different ways to use BIM:

  • Little Closed BIM: The user works on a digital model in his own discipline. He uses one software and does not share his data with other disciplines.
  • Big Closed BIM: Planning participants from different trades deal with a digital model. A common program is used to handle the various disciplines, with data exchange taking place via a proprietary interface.
  • Little Open BIM: The user works on a digital model in his department by means of a single software. Data exchange takes place via a closed and an open interface.
  • Big Open BIM: This variant is the largest possible BIM method. Users from a wide range of disciplines work together on the digital model. Different software solutions are used and data exchange takes place via neutral interfaces.

Conclusion

The BIM planning method makes it possible to work in different variants, each with its own advantages. Open BIM offers users more flexibility, whereas with Closed BIM the interfaces are manageable. Which working method is the right one depends on the type of collaboration and must be determined before the project starts.

What is Little BIM?
Little BIM is an isolated solution. An office or construction company uses one software for only one planning discipline.
What is Big BIM?
Big BIM refers to an end-to-end solution. All project participants within the building life cycle are included.
What is Closed BIM?
Closed BIM is the term for a closed software landscape of only one manufacturer. The data models are proprietary.
What is Open BIM?
Open BIM refers to an open software landscape, solutions from different manufacturers can be used.
What is Little Closed BIM?
In the Little Closed BIM variant, the user from a specialist department uses a digital building model. Software is used and there is no data exchange.
What is Big Closed BIM?
In the Big Closed BIM variant, the planning participants from different disciplines work together on a digital building model. A common software is used and the data exchange takes place via a proprietary interface.
What is Little Open BIM?
With Little Open BIM, the user uses a digital building model in his specialist area. The uniform software landscape enables and simplifies data exchange.
What is Big Open BIM?
Big Open BIM is the largest possible BIM variant. Planning participants from different disciplines work with different software solutions. Data is exchanged via a neutral interface.