Easily share engineering data with friends or colleagues with the PARTcloud.net app
Uploading the photos is easy, and the models are available in different native CAD formats
To share its 3D models with friends or colleagues, users can use the PARTcloud.net 3D Printing & Sharing Community app. Models can be uploaded via PARTcloud.net on the 3D CAD models download portal PARTcommunity in STL and STEP format. With the app, users have access to this data anytime, anywhere.
And this is the way how it works:
- First, users have to login at PARTcloud.net or create an account free of charge in order to enjoy all the advantages of the Sharing Community. If you are already registered for the 3D CAD models download portal PARTcommunity, this is also valid for PARTcloud.net.
- The components are uploaded and the information as well as details filled in so that the 3D CAD model can be found more easily by other users.

- After uploading, the 3D CAD model appears in your own portfolio.

- Now the app PARTcloud.net 3D Printing & Sharing Community by CADENAS has to be installed on the smartphone or tablet.

- In the app itself, the search field is used to enter searched terms - in addition, the two filter functions "newest" and "select a category" can be used.

- Once you have found the 3D model, you have a well-known features, such as downloading the model. In addition, app users have the opportunity to link model and camera function to each other. Thus, two realities can be linked for spectacular photo shots.
Try it out right away: Share and receive 3D CAD models
Whoever is a part of the large Sharing Community will benefit both from the enormous selection of user-generated CAD models and from the platform itself, in order to upload his own models and to make them available to other users.
It's best to go to www.partcloud.net right away and join the Sharing Community
3D CAD models download portal PARTcommunity
If you are in search of manufacturer-certified CAD catalogs, you are at the right place with 3D CAD models download portal PARTcommunity. Look around right away at: www.partcommunity.com
CADENAS - The Innovation Company