Kataloger: 41
3325
Ikke funnet? Be om katalog
Nøkkelord: 228
1100
Enrichments
588
Delivery countries/regions
3
Enheter
3324
File types
3322
Kategorier
1
Klassifiseringer
1
Filter
expansion joint
The expansion joint is a component that is usually used in hydraulics or pneumatics. It is used to connect two pipes or hoses with each other. The sleeve is placed on one of the two pipes and screwed to the other pipe. The expansion joint creates a seal between the two pipes.