Find with 3D Grid Search Example Pipe BendVideosSearch & FindA common thinking error when introducing geometric similarity search products is that engineers have an idea which can be found without any problems. In reality, however, this is not so. The real problem, which is often overlooked, is that an object must first exist in 3D in order to be found at all. But often the creation of such a geometry takes longer than the search.
End Of LifeVideosMechanical Engineer "End of Life" (EOL) and "Product Change Notifications" (PCN) are two important terms used in the manufacturing and electronics industry. They refer to the life cycle of products and the communication of changes to customers or stakeholders.
Digital Twin and important informationIntegration in CAD/PLM/ERPCatalogs & Standards & Company PartsVirtual commissioning (also known as virtual commissioning) is the process of testing a system or plant in a virtual environment before it is put into operation in the real world. The Digital Twin plays an important role in this process.
Provision of master data in several international languagesVideosCatalogs & Standards & Company PartsThere are several reasons why it might make sense to have and prepare master data for engineering in several languages:
Master data enrichment with additional information from ERP / PLMVideosStandardizationMaster data enrichment refers to the process by which a company's master data (basic data) is supplemented with additional information. This can help make data more complete, accurate and relevant to business processes. The sources for enrichment can be internal (from different departments of the company) or external (e.g. from data providers). Here are some steps and considerations to keep in mind when enriching master data with additional information from the company:
Extension of currently not yet existing manufacturer catalogs with crawling and other import proceduresVideosCatalogs & Standards & Company PartsCrawling manufacturer catalogs with 3D CAD models requires specialized techniques and tools, especially if you plan to make regular updates or collect large amounts of data. However, there are several important points to consider before starting a crawling project: