Open-Source Scientific Hardware Made Easy: How Scientists Use 3Dfindit To Accelerate ResearchMechanical Engineering3DfinditA scientific team, led by research engineer Bartosz Zawilski, developed low-cost respiration chambers and openly shared all plans. With 3Dfindit, they quickly found precise CAD models for standard parts, saving time and simplifying documentation.
Engineering talent: How 3Dfindit helped "Dysfunktion" make a breakthroughMechanical EngineeringUniversity & EducationA talented team of young engineers at the University of Cincinnati used 3Dfindit's extensive CAD library to design a 3-pound combat robot with a blade made of titanium.
3Dfindit empowers engineering education and research at the University of Novi SadMechanical EngineeringUniversity & EducationUniversities, colleges and schools worldwide use 3Dfindit as a valuable 3D search engine for their projects and educational purposes.
The 10 largest pump manufacturers in North America Mechanical EngineeringArchitecture EngineeringIn this article, you will learn more about the top 10 pump manufacturers in North America, including industry giants such as Flowserve and Xylem. In addition, the article provides a regional analysis of the locations with the highest concentration of pump manufacturers.
The 10 largest pump manufacturers in Asia Architecture EngineeringMechanical EngineeringThis article presents the 10 leading pump manufacturers in Asia, including their main industries and key markets. In addition, it provides an overview of the Asian countries with the most pump manufacturers - a comprehensive picture of the Asian pump landscape and its major players.
The 10 largest pump manufacturers in Europe KnowledgeMechanical EngineeringThis article highlights the largest pump manufacturers in Europe and provides an insight into the countries with the highest density of pump manufacturers, including Germany, Switzerland, France, the UK and Denmark. Discover which companies dominate the European pump industry.
Application of reversible engineering in 3D reconstruction and selection of sprocketsMechanical EngineeringCADThe thesis on the application of reverse engineering in 3D reconstruction highlights the role of advanced search engines like 3Dfindit, which supports the process by providing comprehensive access to 3D models. Guest post by Marko Zekic
What types of screws are there?Mechanical EngineeringKnowledgeScrews are versatile fasteners that are available in a variety of shapes, materials and sizes and have been specially developed for different applications. In the following article, we look at the types of screws and their areas of application.
What types of pumps are there and when are they used?KnowledgeMechanical EngineeringThere are a variety of pump types that are used depending on the application and requirements. Here is an overview table with some of the most common pump types and their typical applications:
How much does it cost to maintain a digital part?Mechanical EngineeringElectrical EngineeringAny part that can be reused or "standardized" in an assembly can be classified as a "standard part". A standard part can be the assembly of an entire hydraulic system or all the individual parts that make up the system.
Augmented reality in mechanical engineering: the perfect symbiosis?KnowledgeMechanical EngineeringAugmented reality offers users a wide range of possible applications and benefits that are hard to imagine working without these days. AR plays a particularly important role in mechanical engineering and makes a significant contribution to safety, planning and implementation.
The future of manufacturing: Why online platforms are revolutionizing additive manufacturingMechanical EngineeringKnowledgeOnline platforms offer the additive manufacturing industry a wide range of manufacturing options and materials, enabling companies to produce and innovate quickly and cost-effectively.
How do I plan a Hyperloop transportation system?KnowledgeMechanical EngineeringPlanning a Hyperloop transportation system is a complex process that requires extensive technical knowledge, interdisciplinary collaboration and detailed research. Here are some basic steps to consider:
Unitized pistonsProduct ReleasesMechanical EngineeringThe Hallite Type 720 is a ready to fit complete piston.
BearingsProduct ReleasesMechanical EngineeringHallite offer bearings in various types of materials all of which offer high wear-resistance and demonstrate excellent friction properties.
WipersProduct ReleasesMechanical EngineeringWipers are installed in the sealing configurations of hydraulic cylinders to prevent contaminants such as dirt, dust and moisture from entering the cylinder as they retract back into the system.
Piston seals - double acting hydraulic sealsProduct ReleasesMechanical EngineeringPiston seals or piston rings are used in hydraulic cylinders for fluid sealing and are designed to ensure that pressurised fluid does not leak across the piston as the system pressure pushes the piston down the cylinder bore.